Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is a safety shutter and what are its features.
Safety shutter is mounted on the chassis of Easypact MVS/Masterpact NT/NW ACB, the safety shutters automatically block access to the
disconnecting contact cluster when the device is in the disconnected or test positions
(degree of protection IP 20) When the device is removed from its chassis, no live
parts are accessible.

The shutter-locking system is made up of a moving block (optional device) that can
be padlocked (padlock not supplied). The block:
>Prevents connection of the device
>Locks the shutters in the closed position

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.