{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is Anti-Pumping Function provided in Compact NSX 100/160/250/400/630.
The Compact NSX Motor Mechanism Module ON and OFF external inputs can be activated either as a pulse input (at least 1 second) or as a permanent latched supply.

We advise the pulse option as the NSX MT module doesn't have anti-pumping system and if you activate the ON and the OFF inputs at the same time, the MT module will enter in an endless cycle that will damage the MT module.

The client must arrange the installation in order to avoid to send an ON and OFF order at the same time.

For your information, the Masterpact MCH motor mechanism fits an anti-pumping system giving priority to the Open order when you send the Open and Close orders at the same time. But it isn't the case for the NSX MT motor mechanism.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: