Search FAQs
Is it possible to use 3D label ZBY9*2* with XALD/XALK01 ?
The flat surface of the XALK01 is a rectangle 55,3 +/- 0,25 X 59,5 +/- 0,26
The 3D label ZBY9*2* is a circle diameter 60 +/- 0,2
So it could fit but not perfectly
Another option could be to select marked control station:
- Emergency stop XALK01H29
- Arrêt d'urgence XALK01HFR
- Not-Halt XALK01H44
Unfortunately, no other markings for control station
The 3D label ZBY9*2* is a circle diameter 60 +/- 0,2
So it could fit but not perfectly
Another option could be to select marked control station:
- Emergency stop XALK01H29
- Arrêt d'urgence XALK01HFR
- Not-Halt XALK01H44
Unfortunately, no other markings for control station
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: