{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can SturxureWare Data Centre Expert be integrated into Power Monitoring Expert?
For now in PME there isn't dedicated component for DCE integration. The only potential way to bring real-time data from DCE to PME is via OPC or MDI, but nothing as such is mentioned in DCE User Guide or other Manuals.

Further contact with the DCE tech support teams would be needed to confirm if DCE can be run as an OPC DA Server or configured as a Modbus device.

If this is the case then this potential way is possible, and PME can grab real-time data from DCE.

If not then the user needs to add specific devices into PME directly.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.