{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can we combine Easypact MVS with Masterpact NW to make source change over system?

In MVS catalog, we provide only the combination of MVS to build source change over, and don't provide the combination of MVS with NW . MVS design is different from NW, the spring energy is different , so we don't recommend to combine MVS and NW to build source change over.

Schneider Electric Saudi Arabia