Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Why does the S-Flex with bypass not follow deceleration ramp time and freewheel stops instead?
Issue:
Why does an S-Flex with bybass only allow a  freewheel stops instead of rramp?

Product: 
SFD212, S-Flex with Bypass

Environment: 
All

Cause:
Drive will not follow deceleration time. 

Resolution:
SFD212(S-Flex) with bypass will not follow the deceleration time (DEC). This is because when the stop command is given, the drive output contactor (DOC) drops out immediately, causing the run permissive on the R terminal (F112= 1) to drop out and the motor is no longer connected to the VFD. The motor then coasts (freewheel) to a stop. 

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: