Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Video: How to upload Advantys island configuration(STB NIP <example>) through TCP/IP ?

Follow these steps to upload Advantys island configuration(STB NIP <example>) through TCP/IP.
1. Open the Advantys software and provide a new workspace & file name.
2. Go to online > Click connection settings.
3. Select connection type as TCP/IP and enter the IP address of Advantys STB NIP <example> module.
4. Then Click connect > Upload button to start uploading the configuration.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: