Search FAQs
If external ground current transformer is not used with LTMR, is it necessary to connect anything (e.g. resistance) to terminals Z1, Z2 of LTMR?
Issue:
If an external ground current transformer is not being used, is it necessary to connect anything to the Z1 and Z2 terminals of the LTMR?
Product Line:
Tesys T LTMR product line.
Environment:
All situations where an external ground current transformer is not being used.
Cause:
Clarification of product characteristics.
Resolution:
If external ground current transformer is not used, then nothing should be connected to terminals Z1, Z2 of LTMR.
If an external ground current transformer is not being used, is it necessary to connect anything to the Z1 and Z2 terminals of the LTMR?
Product Line:
Tesys T LTMR product line.
Environment:
All situations where an external ground current transformer is not being used.
Cause:
Clarification of product characteristics.
Resolution:
If external ground current transformer is not used, then nothing should be connected to terminals Z1, Z2 of LTMR.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: