{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the ATV320 Compact version I/O terminal card?
Issue:
ATV320 compact version I/O terminal card part number

Product Line:
All Altivar 320 (ATV320) drive part numbers ending with C.

Environment:
N/A

Cause:
Drive has one or more damaged terminals on the control terminal board.  Customer wants to replace the control terminals on an ATV320XXXXC (Altivar 320 Compact) series drive.

Resolution:
The I/O control card part number is VW3A36201.
The book style drive, the one ending with "B" does not need this accessory.

This part is not currently available for sale in the US (as of June 8, 2020).

Schneider Electric Saudi Arabia