Issue:
ATV32 power up with an external 24Vdc supply
Product Line:
ATV32
Environment:
All serial numbers
Cause:
To maintain control power to the drive.
Resolution:
Yes, the P24 terminal and COM are the connections that can be used for external 24VDC.
**NOTE: This does not apply to the ATV320, the P24 terminal on ATV320 is only used to supply the STO (Safe Torque Off) terminal, P24 will not accept 24v.
ATV32 power up with an external 24Vdc supply
Product Line:
ATV32
Environment:
All serial numbers
Cause:
To maintain control power to the drive.
Resolution:
Yes, the P24 terminal and COM are the connections that can be used for external 24VDC.
**NOTE: This does not apply to the ATV320, the P24 terminal on ATV320 is only used to supply the STO (Safe Torque Off) terminal, P24 will not accept 24v.
Released for:Schneider Electric Saudi Arabia