{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to reset variable speed drive Altivar Process locally when controlled over communication?
Whether local means digital input or HMI keys, both are possible.

To reset the fault while the drive is controlled via communication - this can be done:
- either via the same communication channel or
- or it is necessary to switch control temporarily to other channels (e.g. terminals or HMI) and then apply fault reset command from that channel

Case of reset via terminals:
- Configure the same logic input for fault reset and for switching the reference channel (in not separate mode) or switching the command (separate mode).
- Configure the freq channel 2 (in not separate mode) to AI1 , AI2 or AI3 or command channel 2 (separate mode) to terminals.
As soon as you activate digital input, the control channel will switch to a second channel where fault reset is applied at the same time. By releasing the digital input, the control will be reverted back to profinet.

Case of reset via HMI keys:
Configure in menu 5.4 Command and reference - HMI cmd = stop or bumpless
Then by pressing loc/rem key on HMI the drive is switched to HMI control where you can apply reset by pressing the reset key.
Press loc/rem key once again and the control goes back to profinet.

Applicable to other types of communication as well.

Schneider Electric Saudi Arabia