{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the authorized losses levels for transformers in EcoDesign regulation EU 548-2014?
For Oil Distribution and Dry-type transformers (≤ 3150 kVA):
  • Losses levels to be applied (reference of MV ≤ 24 kV and LV ≤ 1.1 kV).
  • ODT and CRT not covered by reference transformers (additional losses allowed compared to standard losses ranges):
  • Medium power and power transformers: Level of Peak Efficiency (Mix of load losses and no load losses) for transformers > 3150 kVA (limited to 10 MVA 36 kV for Dry-type Transformers)
- No losses levels imposed but minimum PEI (Peak Efficiency Index)
- PEI corresponds to:
- the maximum efficiency of the transformer
- Ratio between the no load losses and losses

The values given are Maximal value; no more tolerances on design considered:

Schneider Electric Saudi Arabia