Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the MCS025 Sync-Check module compatible with the SEPAM 40 or 20 series?
Issue
Need to be able to check voltage from another source using the Sepam relay.

Product Line
Sepam 20
Sepam 40
Sepam 80

Environment
Digital relays

Resolution
The MCS025 Sync-Check module only works for the Sepam 80 Series.  It is not compatible with the Sepam 40 or 20 series.  For more information on the MCS025 module, please refer to FA221262.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.