{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the normal service conditions for indoor medium voltage equipment according to IEC 62271-1 concerning ambient?
All MV equipment shall comply with their specific standards.
The IEC 62271-1 standard "Common specifications for high-voltage switchgear and controlgear" defines the normal service conditions for the installation and use of such equipment.

Ambient temperature:
The ambient air temperature does not exceed 40 °C and its average value, measured over a period of 24 h, does not exceed 35 °C.
The preferred values of minimum ambient air temperature are - 5 °C, - 15 °C and - 25 °C.
For instance, regarding pollution, humidity associated with condensation, the standard states:

Pollution:
The ambient air is not significantly polluted by dust, smoke, corrosive and/or flammable gases, vapours or salt.
The manufacturer will assume that, in the absence of specific requirements from the user, there are none.

Humidity:
The conditions of humidity are as follows:
  • The average value of the relative humidity, measured over a period of 24 h does not exceed 95%;
  • The average value of the water vapour pressure, over a period of 24 h does not exceed 2.2 kPa;
  • The average value of the relative humidity, over a period of one month does not exceed 90%;
  • The average value of water vapour pressure, over a period of one month does not exceed 1.8 kPa;
Under these conditions, condensation may occasionally occur.
NOTE 1: Condensation can be expected where sudden temperature changes occur in periods of high humidity.
NOTE 2: To withstand the effects of high humidity and condensation, such as a breakdown of insulation or corrosion of metallic parts, switchgear designed for such conditions should be used.
NOTE 3: Condensation may be prevented by special design of the building or housing, by suitable ventilation and heating of the station or by the use of dehumidifying equipment.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: