{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
'170AEC 920 00'DFB block for Unity

Issue
Provide a DFB block for use with the Unity 'Momentum 170AEC92000' High-speed counter module.

Product Line
Momentum

Environment
Unity

Resolution
If you create a Unity application for a Momentum Unity PLC with a 170AEC92000 module, Unity does not provide a DFB block
for the module.

Th attached DFB can be imported into the Unity application to provide an AEC DFB block for use with the module.  This block was created
by importing a Concept application that contained only the AEC DFB block using Unity 13.

  • Download the attached zip file.
  • Extract the DFB exported file to a temporary folder.
  • Open the Unity application.
  • Right-click on .Dervied FB Types'.
  • Select .Import'.
  • Import the DFB into your Unity application.

zvfbghj

Note:

  • If you decide to create your own DFB block by importing an existing Concept application, Unity 12 must be used as a minimum.

Schneider Electric Saudi Arabia

Attachment(s)
170aec92000 aec dfb.7z [2.63 KB]