Search FAQs
How can I save the public variables of a DFB with PL7-PRO?
The public variables of a DFB can be modified by program or with animation tables. When reloading programs, these public variables return to the initialization values defined in the DFB editor. To retain the modified values, the S box of the variables concerned must be checked (in the DFB editor) and system bit %S94 set to 1. The public variables are then saved.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: