Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the minimum firmware version of the ATV600 drive that is needed to use the VW3A3725 Bacnet card?
Issue:
What is the minimum firmware version of the ATV600 drive that is needed to use the VW3A3725 Bacnet card.

Product Line:
ATV600 series drives.

Environment:
All models, All serial numbers.

Cause:
Drive firmware must be of a certain level to properly operate the VW3A3725 Bacnet card.

Resolution:
A minimum firmware version of V1.8 on the ATV600 series drive is required in order to operate the VW3A3725 Bacnet MS/TP card.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.