{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
If I do not have the Easergy P3 device, how can I create a SCL file for all the signals?
First create an off-line setting file, make sure you select Ethernet port(s) in hardware selection and IEC61850 as Ethernet port protocol. In next step select all signals used to “In use” under Communication/data maps. Then select tool icon and “Export ICD/SCL file…”. Before generation you need to define if RCB names should include indexes (typically selected) and if the file should be in Ed.1 or Ed.2 format. If Edition 2 extensions are selected the file will created in Ed.2 format, otherwise Ed.1 format. When saving the file there is the possibility to save the format as .icd, .iid or .cid.

Schneider Electric Saudi Arabia