Issue:
ATV630 getting an EPF2 Fault after installing the BACnet Card.
Product Line:
ATV600, ATV630, ATV660
Environment:
All
Cause:
NA
Resolution:
Check the Profile Setting. If it is set for I/O profile then change it to Separate or Not Separate. However, changing I/O profile puts you back to factory settings. Therefore, all the VFD settings have to be programmed again.
ATV630 getting an EPF2 Fault after installing the BACnet Card.
Product Line:
ATV600, ATV630, ATV660
Environment:
All
Cause:
NA
Resolution:
Check the Profile Setting. If it is set for I/O profile then change it to Separate or Not Separate. However, changing I/O profile puts you back to factory settings. Therefore, all the VFD settings have to be programmed again.
Released for:Schneider Electric Saudi Arabia