{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What tightening torque has to be applied on the LV429248 6-cable distribution connector for Compact NSX?

Article available in these languages: Czech

The LV429248 connector is designed for 6 cables (Cu or Al) with cross section between 1 and 35 mm².
The tightening torque applied for fixing the cables in the connector are the following:
Cable cross sectionTightening torque
1.5 to 6 (mm²) *4 Nm
8 to 35 (mm²)6 Nm
* For flexible cables from 1.5 to 4 mm², connection with crimped or self-crimping ferrules.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: