{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I activate IRIG-B in Easergy P3 and which modes are supported?
IRIG-B do not need any configuration but the proper hardware must be selected. You need the model with serial port and for Easergy P3 standard the cable REL52826 (VX083) in order to connect the IRIG-B signal. For Easergy P3 advanced you need the communication card with serial port in slot 9 in order to connect the IRIG-B signal to pins 4 and 5.

Easergy P3 support unmodulated mode 003 and 004

Schneider Electric Saudi Arabia