{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

With which devices is the 26997 reference number plug-in base compatible?

The 26997 can be used for installing the C120 and C120NA-DC type of devices with rated current up to 63A.
One plug-in base has to be used per pole.

Schneider Electric Saudi Arabia