{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to add plinth to floor standing Altivar Process variable speed drive ATV630C11N4F?
Floor standing drives ATV630, (ATV630C11N4F) are manufactured in Spacial SF enclosure. Enclosure dimensions of ATV630C11N4F are 400mm (width) and 600mm (depth)
It is possible to add plinth and its references number can be selected from Spacial catalog.
Full catalog downloadable from web (link below)
http://download.schneider-electric.com/files?p_Reference=9993CT0901&p_EnDocType=Catalog&p_File_Id=8636002994&p_File_Name=9993CT0901R08_16%20Body%20(Web).pdf

Anyway, for plinth 100mm high and 400x600mm (widthxheight) you need 1x SYSPF4100 + 1x NSYSPS6100.

Composition of the references can be found on schneider web, see links below

https://www.se.com/us/en/product/NSYSPF4100/spacial-sf-front-plinth---100x400-mm
https://www.se.com/us/en/product/NSYSPS6100/spacial-sf-sm-side-panel-plinth---100x600-mm

Schneider Electric Saudi Arabia