{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is an OHF Fault on an ATV312?
Issue:
ATV312 OHF fault

Product Line:
Altivar, ATV312

Environment:
All

Cause:
Drive over heating fault.
Drive temperature too high

Resolution:
Check the motor load, the drive ventilation and the environment. Wait for the drive to cool before restarting.
Check the see if the cooling fan is running.
The threshold for OHF fault is 118% based on heatsink temp.

Schneider Electric Saudi Arabia