Issue
PLC application is lost on the TSXP57204 after running for 48-72 hours following addition of memory card.
Product Line
Unity, TSXP57204
Environment
Windows 10
Resolution
After 48-72 hours following the adding of a memory card to Premium Unity application that has been running fine for awhile, the
PLC loses the application. The PLC is still powered up.
The reason this could occur may be due to a mechanical problem with the PCMCIA memroy card slot or something internal to the
PCMCIA connector.
If this occurs, it is recommended to replace the PLC.
PLC application is lost on the TSXP57204 after running for 48-72 hours following addition of memory card.
Product Line
Unity, TSXP57204
Environment
Windows 10
Resolution
After 48-72 hours following the adding of a memory card to Premium Unity application that has been running fine for awhile, the
PLC loses the application. The PLC is still powered up.
The reason this could occur may be due to a mechanical problem with the PCMCIA memroy card slot or something internal to the
PCMCIA connector.
If this occurs, it is recommended to replace the PLC.
Released for: Schneider Electric Saudi Arabia




Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.