{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can both M580 redundant power supply modules provide the power at same time and equally
Question:
Can both M580 redundant power supply modules provide the power at same time and equally?

Answer:
No. M580 redundant CPS is designed to have only one active cps providing the power for the sake of life time difference. (or else, It is likely that both CPS fails around the same time which might cause the impact on the customer’s process)

Schneider Electric Saudi Arabia