{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
MiCOM Px4 relays - Dual IP implementation
New MiCOM Px4 relays can have 3 ethernet ports and 2 IP (MAC) interfaces. Depending to the redundancy choice the relation between IP interface and physical ethernet port can be changed.

Attached document is explaining relation between the relay configuration (PRP/HSR or Dual IP) and MAC addressing connection to the physical ports.

It works the same way for hardware with 3 RJ46 and with 1xRJ45 +2xLC.

For more details contact Schneider-Electric Customer Care Centre.

Schneider Electric Saudi Arabia

Attachment(s)
MiCOM Px4 relays - Dual IP implementation.pdf [214.35 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.