Search FAQs
What is a Error 1014 using Somove ?
Issue:
What is a Error 1014 using Somove ?
Product Line:
SoMove software
Environment:
All
Cause:
Getting an Error 1014 when attempting to download program.
Resolution:
Error 1014:
Cannot perform the "Load from Device" operation because some parameter values in the device configuration are not compatible with DTM version.
Troubleshooting:
- install the DTM version which is compatible with the device firmware version (refer the release notes).
- The latest DTM version is available here .
Usually happens due to different firmware versions.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: