{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In SoMove why is "Compare Configurations" grayed out when working with an ATV630 or ATV930?
Issue:
So Move option "Compare Configurations" not working when using ATV630 or ATV930?

Product Line:
Altivar Process Drives

Environment:
SoMove software

Cause:
Unable to compare configurations of Process Drives

Resolution:
It's a known issue, comparing offline two .PSX files is not available for ATV6xx/9xx. This should be fixed in a future SoMove release.
You can make online 'Load from Device and Compare' only, to compare already opened project with the drive

Schneider Electric Saudi Arabia