{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the keypads (HMI's) 'plug-n-play'?
Issue:
Are the HMIs 'plug-and-play'?

Product Line:
All Altivar drives

Environment:
All

Cause:
Would like to know if a drive will automatically detect and use a keypad when connected

Resolution:
Yes, the currently-used keypads with part numbers VW3A1101 and VW3A1111 are 'plug-n-play'. In other words, when you connect the appropriate keypad to an Altivar drive, the drive should automatically detect the keypad. The keypad's LCD screen should display the drive's information almost immediately when connected. This is whether the keypad is plugged directly into the front of the drive or connected by ModBus cable.
VW3A1101                                                     VW3A1111
VW3A1101 VW3A1111



Schneider Electric Saudi Arabia