{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What type of cable can be connected to the A9XPCM04 connector?
To the A9XPCM04 it is possible to connect cable with the following characteristics:
- 35mm² max rigid wires (without ferrule)
- 25mm² max flexible wires (with ferrule)

Schneider Electric Saudi Arabia