{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for a spare side panel for the PX100, Odin battery side car or PDPM144F-M?
Issue:
There is a need to replace a side panel.

Product Line:
NetShelter SX

Environment:
SYMBP100F, PDPM144F-M, SYBSC, SYBSC250K500, SYBSC500K500, all serial numbers.

Cause:
Various issues may require the need for side panel replacement.

Resolution:

The replacement side panel part number is W0M-7171.

Schneider Electric Saudi Arabia