{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can SoMachine controller communicate to a HMI program with Vijeo XD V3.0
Issue:
How do I setup communication between the Controller and HMI and link the variables.

Product Line:
M238, M241, M251, M258
HMIGTO, HMIG3U

Environment:
SoMachine V4.3
Vijeo XD 3.0

Resolution:
Vijeo XD V3.0 is not integrated with SoMachine V4.3
You have to create a separate SoMachine application for the M251 controller and a separate Vijeo XD V3.0 application for the Magelis HMI.

In Vijeo XD, use the SoMachine Network driver under Schneider Electric.  Copy the Node name from the SoMachine application.
Create a symbol link and browse for the application name XML file to import the tags from SoMachine to Vijeo XD.  This file is created during a download in SoMachine.

Schneider Electric Saudi Arabia