undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
MiCOM Px2 relays FAQ. IEC 60870-5-103 ASDU9 measurement implementation.
As described in the standard and user guide the ASDU 9 measures are stored with a rate such as: 2,4 * nominal value = 4096

It means that value is sent as 16 bit were 13 bits (from 3 to 15) corresponds to the analogue value and 3 bits are reserved (from 0 to 3). The full scale for measurement is 240 percent of the nominal equal to 4096.

Example with the relay setting
0104         Frequency                    50Hz
0120         Line CT Primary           1A
0121         Line CT Sec                 1A
0124         Line VT Primary           0.10kV
0126         Line VT Sec                 100.0V

and injection of 0,5A and 98V.

MiCOM Px2 sends following ASDU 9 frame
68 1A 1A 68 08 01 09 09 02 01 A0 94 20 1A 00 00 00 00 30 34 00 00 30 34 50 15 00 00 50 35 3E 16

InjectionNominal valueValue max corresponding to 4096
(In/Un/Pn/Fn*2,4)
Value from deviceValue in 13bitsValue of 13 bits (decimal)Recalculated value as a part of full scale
Ia0,5A1A2,4201Ah
0001101000100
836 (836*2,4)/4096 = 0,4898A
Ua98V100V2403034h
0011010000110
1670(1670*240)/4096 = 97,85V
P 40W40W1x100 = 100W 240240 5015h5015h0001010101010682(682*240)/4096 = 39,96W
F50Hz50Hz1205035h 0011010101010 0011010101010 1706(1706*120)/4096 = 49,98Hz

Where:
Injection – secondary value injected to the relay
Value max – nominal value in the primary or secondary units
Value from device – hexadecimal value send by the IED
Value in 13 bits – conversion from hex to binary with last 3 bits stripped out

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.