Search FAQs
What would cause the ATV600 or ATV900 to show Run 0.0hz if I'm not using anything external to adjust the speed?
Issue:
What would cause the ATV630 to show Run 0.0hz if I'm not using anything external to adjust the speed?
Product Line:
ATV630
Environment:
All
Cause:
Programming
Resolution:
If you're not using an external speed reference (i.e. Potentiometer, Transducer, etc.), when you close 24v to DI1 the drive shows 0.0hz. You will need to go to [Simply Start] set [Low Speed] to 60hz (or desired speed)
What would cause the ATV630 to show Run 0.0hz if I'm not using anything external to adjust the speed?
Product Line:
ATV630
Environment:
All
Cause:
Programming
Resolution:
If you're not using an external speed reference (i.e. Potentiometer, Transducer, etc.), when you close 24v to DI1 the drive shows 0.0hz. You will need to go to [Simply Start] set [Low Speed] to 60hz (or desired speed)
Released for:Schneider Electric Saudi Arabia
Explore more
Category:
Range:
Explore more
Category:
Range: