{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum THDI% permissible for Micrologic 6.0A trip unit equipped with NW12H2-3P-FIXED-85KA?
Thanks to be informed that ,
there is no permissible THD limit for a circuit breaker. The THDi and THDv for networks are generally guided by IEEE 519-2014 and IEC 61000-4-7 standards.

2. Micrologic A trip units do not offer measurements or protections in case of harmonics. In case harmonic measurements and indicators were required, you will have to opt-to Micrologic H. Micrologic H is the only Micrologic trip unit with harmonics measurements capability.

3. Harmonics will generally cause nuisance tripping to all circuit breakers. Thus, when having a harmonics generator in your network, you are advised to use a choke or line reactor to remove/mitigate the harmonics. You can also use passive or active filters in some cases. "

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: