{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What would cause the GV2AF4 adapter not to fit and connect to the ATV320 drive and the GV2 circuit breaker?
Issue:
GV2AF4 connection to ATV320 and GV2 circuit breaker.

Product Line:
ATV320 + GV2 breaker

Environment:
All

Cause:
GV2AF4 adapter pins are not long enough.

Resolution:
There is a newer adapter to connect the GV2 and the ATV320
The new part number is GV2AF5
There is a 29-day lead time on the part so you may need to contact customer service to see if you can expedite the order if needed.
The pins are longer to allow a better connection between the GV2 and the ATV320 drive.

Schneider Electric Saudi Arabia

Attachment(s)
TeSys DF_ LS1-GK1_GV2AF5.pdf [69.87 KB]