Search FAQs
What is the part number for the start- stop kit on 8536 Nema 1 starters with sizes 00, 0, 1, 2 and 3?
Issue:
Needs the part number for the start- stop push button kit on 8536 Nema 1 starters with sizes 00, 0, 1, 2 and 3
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S Contactors and Starters
Cause:
Needs the part number for the start- stop kit on 8536 Nema 1 starters with sizes 00, 0, 1, 2 and 3.
Resolution:
9999SA3
Needs the part number for the start- stop push button kit on 8536 Nema 1 starters with sizes 00, 0, 1, 2 and 3
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S Contactors and Starters
Cause:
Needs the part number for the start- stop kit on 8536 Nema 1 starters with sizes 00, 0, 1, 2 and 3.
Resolution:
9999SA3
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: