Comparison fails when using '.stu' files
Product Line
Unity Dif
Environment
Windows 10
Resolution
If the Unity version installed on the PC is not the same as the Unity version that ws used to create the '.stu' file, the comparison fails.
Unity Diff requires the version of Unity that was used to create the .stu file to also be installed on the PC. The reason for this is because
Unity Dif needs to access the registry entries of Unity, It checks which version is installed and uses Unity to open and converts any other
formatted file to a '.zef' format. Followed by the conversion, it then starts the comparison. If the '.stu' Unity version does not match the
version of Unity installed, it will fail to open the '.stu' file. The failure to open the mismatched Unity version file is a limitation of Unity.
Released for: Schneider Electric Saudi Arabia
Comparison fails when using '.stu' files
Product Line
Unity Dif
Environment
Windows 10
Resolution
If the Unity version installed on the PC is not the same as the Unity version that ws used to create the '.stu' file, the comparison fails.
Unity Diff requires the version of Unity that was used to create the .stu file to also be installed on the PC. The reason for this is because
Unity Dif needs to access the registry entries of Unity, It checks which version is installed and uses Unity to open and converts any other
formatted file to a '.zef' format. Followed by the conversion, it then starts the comparison. If the '.stu' Unity version does not match the
version of Unity installed, it will fail to open the '.stu' file. The failure to open the mismatched Unity version file is a limitation of Unity.
Released for: Schneider Electric Saudi Arabia




Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.