Search FAQs
How and why are Altistart Softstart de-rated for altitude?
Issue:
How and why is the Altistart 48 de-rated for altitude?
Product Line:
ATS48 ATS22 Altistart Softstarts
Environment:
All
Cause:
Wiring
Resolution:
The lower air pressure results in lower air density and so the cooling is less efficient.
There is also a maximum limit. This is due to the reduced air electrical resistance, which requires larger spacing to prevent arcing. The circuit boards and component spacing allows only a certain altitude and you can’t install it higher.
Maximum Operating Altitude;
How and why is the Altistart 48 de-rated for altitude?
Product Line:
ATS48 ATS22 Altistart Softstarts
Environment:
All
Cause:
Wiring
Resolution:
The lower air pressure results in lower air density and so the cooling is less efficient.
There is also a maximum limit. This is due to the reduced air electrical resistance, which requires larger spacing to prevent arcing. The circuit boards and component spacing allows only a certain altitude and you can’t install it higher.
Maximum Operating Altitude;
3300 ft (1000 m) without de-rating. Above this, de-rate the
nominal current by 2.2% for each additional 330 ft
(100 m) to a maximum of 6600 ft (2000 m)Released for:Schneider Electric Saudi Arabia
Explore more
Category:
Explore more
Category: