{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the power consumption of a PTC probe wired to the LT3SM protection relay ?

The current flown via the PTC probe is 1-2mA
2mA is flown at low temperature (PTC probe has low resistance)
1mA is flown at high temperature (PTC probe has high resistance)
If PTC probe will be tempoary replaced by resistor 250 Ohms (simulates low temperature) its power consumption will be I^2*R = 2mA * 2mA * 250 Ohms = 1 mW

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: