{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you configure a relay output on ATV630/930 to indicate safety input status?
Issue:
The Altivar Process ATV630 and ATV930 needs a relay to indicate if the safety input is active or not active.

Product Line:
ATV630, ATV930

Environment:
All serial numbers, all model numbers

Cause:
Need for an indication of the safety circuit status on STOA / STOB input terminals.

Resolution:
Configure one of the relays of the drive to "Power Removal State":
  • Go to Complete Settings
  • Go to Input/Output Relay
  • Go to Rx Configuration
  • Set Rx assignment to "Power Removal State"

Replace x with the number of the relay you want to use.

Schneider Electric Saudi Arabia