{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the ATV340 have programmable logic functions like the ATV32 and ATV320?

Article available in these languages: Spanish

Issue:
Wondering if the ATV340 drives have programmable logic functions, like the ATV32 and ATV320?

Product Line:
ATV 340

Environment:
All

Cause:
Configuration

Resolution:
The ATV32 and ATV320 have logic functions that you can program via SoMove.  The ATV340 is configured like the ATV630 and the ATV930, so the answer is No, there is no internal logic.

Schneider Electric Saudi Arabia