{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the specifications of PT/KTY/PTC that can be used on the ATV630 process drive?
Issue:
PT/KTY/PTC specifications that can be used on the ATV630 process drive.

Product Line:
Altivar 630, Process

Environment:
All

Cause:
N/A

Resolution:
AI2-AI3 Sensor inputs I Software-configurable PT100/PT1000 or KTY84 or PTC or Water level
sensor
PT100
1 or 3 thermal sensors mounted in series (configurable by
software)
Sensor current: 5 mA
Range –20/200°C
Accuracy +/– 4°C for a temperature variation of 60°C

Schneider Electric Saudi Arabia