{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the function of BSCM Module and how to Setting Up it?
The BSCM module (Breaker Status & Control Module) can be used to send the following data via the communication bus:
 Device states (feedback from OF, SD and SDE contacts)
 Control instructions for the communicating motor mechanism (opening, closing and resetting)
 Information to assist the operator (storage of the last 10 events)

This module can be used with all Compact NSX circuit breakers equipped with thermal-magnetic and Micrologic electronic trip units and with all Compact NSX switches.
The BSCM module must always be used:
 With the NSX cord
 When the communicating motor mechanism has been installed

Setting Up the BSCM Module:
Setting up the BSCM module on the communication bus requires no addressing.
LED indication on the BSCM module confirms that the BSCM module is working.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.