Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What demand parameters are available in PM1130H meter ?
The meter provides last, present, and maximum (peak) demand values, and a
timestamp through counters when maximum (peak) demand occurred.
The meter supports standard demand calculation methods, including sliding block,
fixed block, and rolling block.
Peak demand registers can be reset manually (password protected) or through
communication.
Demand measurements include:
• Demand (Total): W, VAR, VA

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: