Search FAQs
Unable to add elements to Logipam (SFT2885) ladder logic diagram
Issue
Customer is unable to add elements to a Logipam (SFT2885) diagram using click and drag
Product Line
Logipam (SFT2885)
Sepam 80 Series
Environment
Logipam (SFT2885)
Customer is unable to add elements to a Logipam (SFT2885) diagram using click and drag
Product Line
Logipam (SFT2885)
Sepam 80 Series
Environment
Logipam (SFT2885)
Cause
SFT2885 must be reinstalled
Resolution
1) Uninstall SFT2885
2) Download Setup SFT2885 V3.3.exe from Logipam SFT2885 V3.3 Download
3) Run Setup SFT2885 V3.3.exe to complete the reinstallation*
* A restart may be required to complete the installation
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: