{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
When using flange kits, what is the ATV630/930 depth dimension inside and outside the enclosure?
Issue:
ATV630/930 depth dimension inside and outside the enclosure when usinf a flange kit

Product Line:
ATV630 ATV930

Environment:
All mounted with flange kit

Cause:
Installation clearances

Resolution:
The flange kit allows the heatsink to protrude out the back of an enclosure. The VFD depth inside and outside of the enclosure is important for clearances.
See the attached file.

A is outside of enclosure
B is inside enclosure

Schneider Electric Saudi Arabia

Attachment(s)
Dimension pictorial.pdf [51 KB]