{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the NetShelter CX PDU (AP9567 or AP9568) be plugged into a higher amp power source? Will it protect the fans?
Issue:
A customer asks if it's safe to connect the 10A NetShelter CX PDU into a higher amperage port on a UPS or PDU. They want to make sure the fans are protected.

Product Line:
NetShelter CX

Environment:
All models, all serial numbers.

Cause:
A customer may have a UPS or PDU that only offers ports with higher Amp ratings than that of the PDU.

Resolution:
Yes, the PDU can be connected into a port with a higher Amp rating.
An example of this would be that in North America it's ok to connect the NEMA 5-15P on the end of the AP9567 power cord into a NEMA 5-20R receptacle on a PDU or UPS.

Schneider Electric Saudi Arabia