{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many BMXEIA0100 (AS-interface module) can be configured in a M580 architecture?
Issue

How many BMXEIA0100 can be used in a M580 architecture?

Product Line

M580, BMXEIA0100

Resolution

16 is the max number of BMXEIA0100 AS-i modules accepted in M580 configuration. This is the global limitation for the M580 system.
With have other limitations on drops & local CPU rack:
=> 2 max on RIO drops with CRA
=> 2 max on level 10 CPU, 4 max on level 20, 6 on level 30 and 8 for above.


Schneider Electric Saudi Arabia